Dashboard
-
HiLCOS 10.12 Release Update 12 (10.12.7389)
Improvements in HiLCOS 10.12.7153-RU12
-
Provize Suite 01.7.00 released
Version 01.7.00 of the BELDEN Provize Suite has just been released and is available for download now: Windows: https://hirschmann-support.belden.com/downloads/files/4081-provizesuite-latest-windowsexedownloadzip
-
HiSecOS v04.8.00 released
Software Release 04.8.00 ------------------------ Bugfixes (Refer Issue List) New features supported: - E3.LOG.011: Logs download in CSV format - E3.PMON.008: Fast link flap Security Fix: - OpenSSL upgraded to 1.1.1w - Busybox upgraded to 1.36.1 - Dbus upgraded to 1.14.8 -...
-
Classic Switch v09.1.11 released
Software Release 09.1.11 ------------------------ Bugfixes (see issuelist)
-
Industrial HiVision 08.5.00 and HiFusion 04.5.00 released
Industrial HiVision 08.5.00 and HiFusion 04.5.00 were released. You can find them in the download area from now on!
-
Industrial HiVision 08.5.00 released
Issues fixed You can find the known problems, workarounds, fixes and java-vulnerabilities corrected in the issue list.
-
Provize Suite 01.6.02 released
Version 01.6.02 of the BELDEN Provize Suite has just been released and is available for download now: https://hirschmann-support.belden.com/downloads/files/4081-provizesuite-latest-windowsexedownloadzip
-
HiOS 07.1.09 has been released
HiOS 07.1.09 was released for the following devices: GRS1020/30
-
HiEOS 01.0.01 released
This is the first software bugfix release for the HiEOS software for the LRS device family.
-
Provize Suite 01.6.01 was released!
Issues fixed You can find the problems, workarounds and fixes related to this release in the issue list.Version 01.6.01 Issue with the UI language has been fixed and German is available again.
-
See all news
- When or why should I configure ""Compatibility to RFC 1583""?
- How can I configure a Virtual Link crossing an NSSA?
- Introduction - What redundancy solutions are there? Which should I use? What do I have to consider?
- Configuring PTP in Hirschmann Switches for use with Kinetix 5700 Drives
- Americas - RMA Request Instructions