Skip to main content

Application Note - OWL User Module - Tailscale - Knowledgebase / Products / OWL / User Modules - Hirschmann Support Center

Application Note - OWL User Module - Tailscale

User Module Description

The user module “Tailscale” allows you to easily connect to the OWL router or IP devices attached to it. It provides a convenient way to run the Tailscale[1] client on the OWL router.

This module requires the CA Bundle user module to be installed as well! If the Tailscale module gets installed afterwards please restart the device. Please install at least CA Bundle 1.0.1