Paessler AG's PRTG Network Monitor is a common tool to observe the status of many network devices. This guide will help you to quickly connect Hirschmann BAT (HiLCOS) devices such as:
- BAT-R, BAT-F
- BAT450-F
- BAT867-R, BAT867-F
Please be aware that monitoring devices excessively can take performance away from them as well as cause additional traffic on the network. Especially in critical applications and when monitoring devices over a WLAN connection instead of a switched infrastructure. This can cause degradation of the application performance that would not be there without monitoring. We tuned the default intervals for the example sensors for a typical system, but you should check and rework these settings according to your application and requirements.