This lesson explains the IGMP Proxy configuration. This feature is available on HiOS 3S devices.
IGMP Proxy is a router function to forward MC streams in an easy way on devices without MC routing capabilities.
Scenario

IGMP is needed on the consumer interfaces so the router collects joins from the consumers.
IGMP Proxy then forwards the joins to the interface where the producer is located.
With IGMP Proxy MC streams can be forwarded in one direction only.
Router Interface Configuration

Example router interface configuration
IGMP Configuration

Enable IGMP on the interface where the consumer is connected
IGMP Proxy Configuration

Enable IGMP Proxy on the port pointing to the multicast producer.
Repeat the steps in case you have multiple devices in a chain.