Tableau de bord
-
Industrial HiVision 08.5.00 and HiFusion 04.5.00 released
Industrial HiVision 08.5.00 and HiFusion 04.5.00 were released. You can find them in the download area from now on!
-
Industrial HiVision 08.5.00 released
Issues fixed You can find the known problems, workarounds, fixes and java-vulnerabilities corrected in the issue list.
-
Provize Suite 01.6.02 released
Version 01.6.02 of the BELDEN Provize Suite has just been released and is available for download now: https://hirschmann-support.belden.com/downloads/files/4081-provizesuite-latest-windowsexedownloadzip
-
HiOS 07.1.09 has been released
HiOS 07.1.09 was released for the following devices: GRS1020/30
-
HiEOS 01.0.01 released
This is the first software bugfix release for the HiEOS software for the LRS device family.
-
Provize Suite 01.6.01 was released!
Issues fixed You can find the problems, workarounds and fixes related to this release in the issue list.Version 01.6.01 Issue with the UI language has been fixed and German is available again.
-
HiOS 07.1.08 has been released
Software Release 07.1.08 ------------------------ Bugfixes (see Issue List)
-
HiLCOS 10.34 Release Update 6
Overview on new features as of version 10.34.6201-RU6WLAN Diagnostic Log additions • Receive signal strength information about neighbor access points is additionally provided in WLAN-Diagnostics Log. The presented information on signal strength is equivalent to the WLAN-STRENGTH trace information. • A new...
-
Classic Switch v09.1.10 released
Software Release 09.1.10 ------------------------ Bugfixes (see issuelist)
-
Provize Suite 01.6.00 was released!
A new release of Belden Provize Suite is available - version 01.6.00 was released and is now available for download. Release Notes:Issues fixed You can find the problems, workarounds and fixes related to this release in the issue list.Version 01.6.00...
-
Voir toutes les actualités
- When or why should I configure ""Compatibility to RFC 1583""?
- How can I configure a Virtual Link crossing an NSSA?
- Introduction - What redundancy solutions are there? Which should I use? What do I have to consider?
- Configuring PTP in Hirschmann Switches for use with Kinetix 5700 Drives
- Americas - RMA Request Instructions