跳到主要内容

What are the allowed characters for user passwords? - 知识库 / Products / HiOS - Belden Support Center

What are the allowed characters for user passwords?

ASCII characters between 'space' and 'z' which is HEX 20 to HEX 7A except HEX 22 (double quotes "") .
This means A ... Z, a ... z, 0 ... 9
and the following special characters: !#$%&'()*+,-./:;<=>?@[\]^_`{}~