Zum Hauptinhalt springen

Classic Firewall v05.3.05 released - Neuigkeiten / Firewalls - Belden Support Center

März 13 2019

Classic Firewall v05.3.05 released

- Corrections:

    Modified serial number of ACA 21 (new) and ACA 22 is shown in CLI using command "show system info",

    Correct accuracy of internal clock,

    Successive authentication list methods are not processed if previous method returned a reject,

    Firewall forwarding EAPoL frames for 802.1X when specific Firewall rules and EAPOL are enabled

- EAPOL configuration option under Port Forwarding is shown in CLI using command "show packet-forwarding" as well as in GUI