Zum Hauptinhalt springen

Industrial HiVision 08.5.00 released - Neuigkeiten / Software Products - Belden Support Center

März 21 2024

Industrial HiVision 08.5.00 released

Issues fixed

  • You can find the known problems, workarounds, fixes and java-vulnerabilities corrected in the issue list.


FAQ (Frequently Asked Question)


New features in version 08.5.00

  • New Devices

    • Hirschmann IT DAP847

Additions to the manual in version 08.5.00

  • Hirschmann IT Family

    • MTS Family: In the default setting the LLDP and SNMP functions are disabled on the device. To have Industrial HiVision discover and display these devices, enable the LLDP and SNMP functions.

    • DAP847: In the default setting the LLDP and SNMP functions are disabled are disabled on the device. To have Industrial HiVision discover and display these devices, enable the LLDP and SNMP functions. Additionally, the Wifi connection are not displayed by the Auto-Topology function.