Ir al contenido principal

Are there sofware-restrictions when running Industrial HiVision on Windows Server installations? - Base de conocimiento / Products / Industrial HiVision - Belden Support Center

Are there sofware-restrictions when running Industrial HiVision on Windows Server installations?

The following restrictions must be taken into account when running Industrial HiVision on a (supported) Windows Server operating system:

  • Windows Server 2008 R2 (or later)
    Do not use as a Windows server:
    Share Point Services, Exchange Server and Active Directory should not be installed.

This information is also present in the readme of Industrial HiVision. Please always check the readme of your installation, if there are any further restrictions for your installed version of Industrial HiVision. You can find the readme under "Help" --> "Readme" from your Industrial HiVision user interface.