Can the BAT-C transfert tagged frames transparently in a environment with VLANs ? - Base de conocimiento / Products / Discontinued Products / BAT-C - Belden Support Center
Can the BAT-C transfert tagged frames transparently in a environment with VLANs ?
No, In spite of the tagged frames are accepted on both interfaces (LAN and WLAN), the outgoing traffic on the LAN interface is always sent untagged. It means that the VLAN information is lost.