Ir al contenido principal

Using Radius to access Switch Agent (HiOS/HiSecOS - RSP, MSP,EAGLE) - Base de conocimiento / Products / HiSecOS - Belden Support Center

Using Radius to access Switch Agent (HiOS/HiSecOS - RSP, MSP,EAGLE)

 

This lesson describes how to configure radius for switch management access via telnet and webinterface on devices running HiOS and HiSecOS.

Configure Radius-Server

1.) Click on "Create" and enter IP-address of Radius-Server.
2.) Configure "Shared Secret". Please note that this field will be empty after the next step because of security reasons.
3.) Click on "Set" in order to send new configuration to switch agent.

Optional: Use CLI

Please use following command:

radius server auth add 1 ip <ip-address>
radius server auth modify 1 secret

Configure Authentication List

1.) Configure "defaultLoginAuthList" and insert "radius" as a policy.
2.) Click on "Set" in order to send new configuration to switch agent.

Optional: Use CLI

Please use following command:

authlists set-policy defaultLoginAuthList local radius

 

Radius Configuration

Service-Types

Service-Type := Administrative-User „admin“
Service-Type := Login-User „operator“
Service-Type := NAS-Prompt-User „user“
No Service-Type reject login