Ir al contenido principal

Classic Switch v09.0.18 released (MACH1040 and MACH 104) - Noticias / Switches and Router - Belden Support Center

may 20 2019

Classic Switch v09.0.18 released (MACH1040 and MACH 104)

Classic Switch software 09.0.18 has been released for MACH 1040 and 104.
This version fixes a link issue in cobination with SFPs:

In certain scenarios when unplugging a fiber link from a port also the neighbor port is going down