Ir al contenido principal

HiFusion v03.1.00 released - Noticias / Software Products - Belden Support Center

dic 5 2017

HiFusion v03.1.00 released

New features in version 03.1.00

  • Generates PSMs compatible with Ind. HiVision 07.1.00.

Fixes in version 03.1.00

  • The feature 'GPS Coordinates of a device' can be disabled, but property always appears in Ind. HiVision.
    Fix: Feature cannot be disabled any more.
  • If in one PSM different device icons were defined for different Sys OIDs it could happen, that all devices got the same icon.
    Fixed.
  • Management protocols: The 2 checkboxes 'HTTP' and 'HTTPS' were replaced by the checkbox 'Web Interface'.
    Ind. HiVision determines which version to use.
  • The feature 'Signaling' was present in HiFusion. Only Hirschmann devices support Signaling.
    Fix: Feature was removed from HiFusion.