Ir al contenido principal

HiSecOS 05.1.00 has been released - Noticias / Firewalls - Belden Support Center

oct 8 2024

HiSecOS 05.1.00 has been released

Software Release 05.1.00

------------------------

Bugfixes (Refer Issue List)

New features supported:

- E3.DPI.008: Goose Enforcer

Security Fix:

- OpenSSH upgraded to 9.8p1

- libexpat upgraded to 2.6.2

Open points and decisions:

- FDB: After adding static mac address to interface-1, same mac is getting

learned to other interface-2 while traffic is send with same mac as source

mac on interface-2

- Eagle web become unresponsive, once web remain open for more than a day

- After creating around 1000 L2 filter rule via CLI, web of L2 filter rule

gives error to contact to manufacturer


This software release 05.1.00 is released exclusively for the following hardware:

HiSecOS-eagle4007-05100.bin:

- EAGLE40-5TX/2SFP (from serial number 942300101xxxxxxxxx)

- EAGLE40-5TX/2SFP-EEC (from serial number 942300102xxxxxxxxx)

- EAGLE40-5TX/2SFP-EEC-IN (from serial number 942300103xxxxxxxxx)