Passer au contenu principal

HiOS v07.2.02 released - Actualités / Switches and Router - Belden Support Center

déc. 18 2018

HiOS v07.2.02 released

This platform software release 07.2.02 is released exclusively for the 

following hardware:


HiOS-DRAGON-07202.bin:

- DRAGON-00484           (Since SW 07.2.00)

- DRAGON-00808           (Since SW 07.2.02)


Supported Software Level / Packages:

- 2A

- 3A UR (Unicast Routing)

- 3A MR (Unicast + Multicast Routing)