Dashboard
-
OpEdge-8D v01.0.04 released
New Features: Enhanced connectivity has been introduced to link the Gateway with the Belden Horizon On-Premises server. The following functionalities are now available: Activation and management of the Gateway. Support for SRA and PDN tunnels. Deployment of container applications. Shell...
-
HiEOS 01.1.00 released
Software Release 01.1.00 ------------------------ Minor (see Issue List)
-
HiOS 09.4.03 released
Software Release 09.4.03 ------------------------ Bugfixes (see Issue List)
-
Provize Suite 01.7.01 released
Version 01.7.01 of the BELDEN Provize Suite has just been released and is available for download now: Windows: https://hirschmann-support.belden.com/downloads/files/4081-provizesuite-latest-windowsexedownloadzip
-
HiLCOS 10.12 Release Update 12 (10.12.7389)
Improvements in HiLCOS 10.12.7153-RU12
-
Provize Suite 01.7.00 released
Version 01.7.00 of the BELDEN Provize Suite has just been released and is available for download now: Windows: https://hirschmann-support.belden.com/downloads/files/4081-provizesuite-latest-windowsexedownloadzip
-
HiSecOS v04.8.00 released
Software Release 04.8.00 ------------------------ Bugfixes (Refer Issue List) New features supported: - E3.LOG.011: Logs download in CSV format - E3.PMON.008: Fast link flap Security Fix: - OpenSSL upgraded to 1.1.1w - Busybox upgraded to 1.36.1 - Dbus upgraded to 1.14.8 -...
-
Classic Switch v09.1.11 released
Software Release 09.1.11 ------------------------ Bugfixes (see issuelist)
-
Industrial HiVision 08.5.00 and HiFusion 04.5.00 released
Industrial HiVision 08.5.00 and HiFusion 04.5.00 were released. You can find them in the download area from now on!
-
Industrial HiVision 08.5.00 released
Issues fixed You can find the known problems, workarounds, fixes and java-vulnerabilities corrected in the issue list.
-
Alle Neuigkeiten anzeigen
- When or why should I configure ""Compatibility to RFC 1583""?
- How can I configure a Virtual Link crossing an NSSA?
- Einführung - Welche Redundanzlösungen gibt es? Welche soll ich benutzen? Was muss ich beachten?
- Configuring PTP in Hirschmann Switches for use with Kinetix 5700 Drives
- Americas - RMA Request Instructions