Overslaan naar hoofdinhoud

Provize v1.0 released - Nieuws / Software Products - Belden Support Center

aug 31 2020

Provize v1.0 released

Provize v1.0, the next generation network management software from Belden, is now available for download. This free of charge first version has limited functionality, and was created to validate the underlying architecture and the user interface.


Functions include:

  • Device discovery
  • Guided Installation
  • Initial Password Change
  • LLDP based topology creation
  • Topology diagrams of devices and connections
  • Device availability using ping


You can download a software bundle containing the installers for Windows and Linux operating systems here:

https://hirschmann-support.belden.com/downloads/files/2853