Ir para o conteúdo principal

Can I supervise the optical transmit and receive levels at fix mounted transceivers (not SFPs), e.g. using SNMP? - Base de Conhecimento / Products / HiOS - Belden Support Center

Can I supervise the optical transmit and receive levels at fix mounted transceivers (not SFPs), e.g. using SNMP?

No, this is not possible.
The fix mounted transceivers do not measure optical transmit or receive power.