Ir para o conteúdo principal

HiOS device: Which TLS version is supported by the email client? - Base de Conhecimento / Products / HiOS - Belden Support Center

HiOS device: Which TLS version is supported by the email client?

HiOS devices of release 7 support TLS v1.0 and 1.2. Release 1.1 is not supported, because it doesn't offer much more than 1.0.
By GUI you can either select no or TLS v1.0/1.2 encryption.