Ir para o conteúdo principal

How can I start HiView as external application? - Base de Conhecimento / Products / Industrial HiVision - Belden Support Center

How can I start HiView as external application?

 

Starting HiView using the AppletLauncher.exe with the option -address allows to start HiView as external application from HiDiscovery and Industrial HiVision.

HiDiscovery PreferencesCopy link to HiDiscovery Preferences to clipboard

To use HiView instead of a web browser from HiDisovery you need to change the web browser path to <install-dir HiView>\AppletLauncher.exe -address

If you then highlight one device and click on WWW, HiView will start and open the selected device's webinterface

Industrial HiVision PreferencesCopy link to Industrial HiVision Preferences to clipboard

To use HiView instead of a web browser from Industrial HiVision you need to change the browser path to <install-dir HiView>\AppletLauncher.exe -address

If you then select web interface from a device's context menu, HiView will start and open the selected device's webinterface.