Ir para o conteúdo principal

IHV Audit Trail - Linux - Base de Conhecimento / Products / Industrial HiVision - Belden Support Center

IHV Audit Trail - Linux

As of v6.0 IHV logs events to the Linux SysLog.
The events include:

  • Log in and out of Industrial HiVision
  • Any action which results in an SNMP Set Request being sent to a device, including the MIB variable that was set, and the new value
  • Any actions from HiDiscovery within Industrial HiVision
  • Start of external applications
  • All actions for which the "Edit Mode" is needed

 

Edit syslog.conf

In this example it is rsyslog.conf file present in /etc/ folder
Edit/uncomment the following lines:

  1. provides UDP syslog reception
    $ModLoad imudp
    $UDPServerRun 514

Restart rsyslogd in order to apply the changes

 

SysLog File

tail -f /var/log/syslog |grep Industrial