Ir para o conteúdo principal

IP/MAC pairs - Base de Conhecimento / Products / Industrial HiVision - Belden Support Center

IP/MAC pairs

IP/MAC pairs is a security feature which is available as of IHV v6.0.
The purpose of this feature is to maintain a list of IP-MAC pairs and to signal if address associations change.


Select Configuration - MAC/IP List from the menu to open the current list of address pairs.

 

 MAC/IP address pair list

Change to the tab MAC/IP Address Pair Security.

IP/MAC pairs contained by this list will be differentiated between three types:

  • Existent (in field)
  • User generated (they are manually added by the user using add functionality or by selecting one of the existent pair and edit it).
  • Excluded/Excepted (these are also added by user manually or by selecting and editing/converting an existent record. These do not preserve the MAC Address. For them will never be raised a warning event.
    If Configure Schedule for Checking is checked the scheduler dialog will appear on leaving this dialog.

  

Scheduler

In this dialog you can specify the schedule for checking IP/MAC pairs.
The minimum interval for this feature is 30 minutes.

 

Log Message