Ir para o conteúdo principal

Which Hirschmann devices support HIPER Ring over LAG? - Base de Conhecimento / Products / Classic Switches - Belden Support Center

Which Hirschmann devices support HIPER Ring over LAG?

HIPER Ring over LAG is supported by PowerMICE and all MACH 4000. Including Platform 4 release 8.0.x there is no other device supporting HR over LAG, and there is nothing planned.

Platform 5 devices do not support HIPER Ring.