Ir para o conteúdo principal

HiOS 08.9.00 released - Notícias / Switches and Router - Belden Support Center

out. 29 2021

HiOS 08.9.00 released

1. Limitations of the release GRS106 08.9.00
==============================================

USB-C: The Out-of-Band management interface exclusively supports CLI access via
terminal emulation.


2. Supported Hardware
=====================
This platform software release 08.9.00 is released exclusively for the
following hardware:

HiOS-GRS-08900.bin:
- GRS105-6F8F16T (Since SW 08.9.00)
- GRS105-6F8T16T (Since SW 08.9.00)
- GRS106-6F8F16T (Since SW 08.9.00)
- GRS106-6F8T16T (Since SW 08.9.00)


Supported Software Level:
- 2S (GRS...2S, GRS...2A)
- 2A (GRS...2A)

For information on supported accessories, refer to the "User Manual Installation".
You will find the manuals under "https://www.doc.hirschmann.com".

3. History of Changes
=====================

Software Release 08.9.00
------------------------
First Version

New Functions:
- Humidity Sensor
- Responsive GUI