Ir para o conteúdo principal

HiOS v08.3.00 released for Octopus - Notícias / Switches and Router - Belden Support Center

jun. 26 2020

HiOS v08.3.00 released for Octopus

Software Release 08.3.00
------------------------
Only available for HiOS-OCTOPUS-IPv6-08300.bin.

New Functions:
- IPv6 management
- BOOTP/DHCP options (DHCP client) can be switched off.
- Display delivered PoE current in mA (additional to the power in W).

Software Level 2A:
- Display differences to default configuration in the graphical user interface.
- New parameter "index" in the CLI for adding and deleting ACL rules.