Ir para o conteúdo principal

HiOS v08.4.01 released - Notícias / Switches and Router - Belden Support Center

set. 11 2020

HiOS v08.4.01 released

Software Release 08.4.01
------------------------
Bugfixes (see Issue List)

New Functions:
- Maximum number of configurable static routes increased from 512 to 1280.
- BOOTP/DHCP options (DHCP client) can be switched off.
- Display differences to default configuration in the graphical user interface.
- New parameter "index" in the CLI for adding and deleting ACL rules.