Ir para o conteúdo principal

Provize Suite 01.9.01 and Classic Webview 01.0.01 released - Notícias / Software Products - Belden Support Center

out. 21 2024

Provize Suite 01.9.01 and Classic Webview 01.0.01 released

Issues fixed

Version 01.9.01

New features in Provize® Suite

You can find the following new features in this version.

  • Suite - Provize® Classic WebView. Provize® Suite requires Provize® Classic WebView to open the web interface of Classic devices. The installation steps for Provize® Classic WebView no longer include an installer. Refer to the readme or the Open Web Interface chapter of the Provize® Suite help guide for further information on the installation of Provize® Classic WebView.