As of HiMobile version 2.0 next to devices also network connections and their properties are available.
HiMobile Home Screen
![](/file.php/6BNXQWCDJWW528875B665/IMG_1185.png)
Click on Network to browse the project tree.
Project / Folders
![](/file.php/6JBJTZSTDRB5289227524/media_1429866552023.png)
Select a project and subfolder to display the device/connections list.
The connections can be found below the device list.
Select one to display the connection properties.
There are two screens. Wipe left/right to change between them.