Ir al contenido principal

HiSecOS v04.1.01 released - Noticias / Firewalls - Belden Support Center

jun 9 2021

HiSecOS v04.1.01 released

Software Release 04.1.01
------------------------
New Feature supported:
-L2 Stateful Firewall on EAGLE40

Security Fix:
None

Open points and decisions:
 - FDB: After adding static mac address to interface-1, same mac is getting learned to other interface-2 while traffic is send with same mac as source mac on interface-2
 - No support of copper SFP in device, it might work with hot plug in and port goes down after reboot
 - Eagle web become unresponsive, once web remain open for more than a day
 - Vlan tagged packet not getting filtered by l2 filtering if matched on vlan interface with untagged egress port
 - After creating around 1000 L2 filter rule via CLI, web of L2 filter rule gives error to contact to manufacturer