Ir al contenido principal

HiSecOS v04.5.00 released - Noticias / Firewalls - Belden Support Center

abr 20 2023

HiSecOS v04.5.00 released


Software Release 04.5.00
------------------------
Bugfixes (Refer Issue List)

New features supported:
 - E3.TSYNC.005 Day Light Saving

Security Fix:
 - uClibC upgraded to 1.0.42
 - Multiple security issues fixed

Open points and decisions:
 - FDB: After adding static mac address to interface-1, same mac is getting
learned to other interface-2 while traffic is send with same mac as source
mac on interface-2
 - Eagle web become unresponsive, once web remain open for more than a day
 - After creating around 1000 L2 filter rule via CLI, web of L2 filter rule
gives error to contact to manufacturer