This lesson describes the feature Dashboard which was introduced with HiMobile v3.0.
Network Dashboard
![](/file.php/6NDDBRPSXCK527886D026/01_media_1495013999576.png)
In the HiMobile home screen, tap the „Dashboard“ icon to get a summary of all devices and connections in the network, categorized by their status
Dashboard View
![](/file.php/6HQPJGDZBWP5280B0ABB8/02_media_1495014035912.png)
Beside the number of errors, warnings and ok you can also see how many devices and connections have this status.
Dashboard Refresh
![](/file.php/6YYQXGWHXAP52819122CA/03_media_1495014921629.png)
The dashboard can be manually refreshed by tapping on the 3 dots in the upper right corner and select "Refresh"