Passer au contenu principal

Industrial HiVision 08.1.00 was released - Actualités / Software Products - Belden Support Center

déc. 20 2019

Industrial HiVision 08.1.00 was released

Security Vulnerability Corrected in version 08.1.00

                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                               

VulnerabilityDescription
Java CVE-2019-2933Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE                 (component: Libraries). Difficult to exploit vulnerability allows unauthenticated attacker with network access via                 multiple protocols to compromise Java SE, Java SE Embedded. Successful attacks require human interaction from a person                 other than the attacker. Successful attacks of this vulnerability can result in unauthorized read access to a subset of                 Java SE, Java SE Embedded accessible data.
Java CVE-2019-2945Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE                 (component: Networking). Difficult to exploit vulnerability allows unauthenticated attacker with network access via                 multiple protocols to compromise Java SE, Java SE Embedded. Successful attacks require human interaction from a person                 other than the attacker. Successful attacks of this vulnerability can result in unauthorized ability to cause a partial                 denial of service (partial DOS) of Java SE, Java SE Embedded.
Java CVE-2019-2958Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE                 (component: Libraries). Difficult to exploit vulnerability allows unauthenticated attacker with network access via multiple                 protocols to compromise Java SE, Java SE Embedded. Successful attacks of this vulnerability can result in unauthorized                 creation, deletion or modification access to critical data or all Java SE, Java SE Embedded accessible data.
Java CVE-2019-2962Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE                 (component: 2D). Difficult to exploit vulnerability allows unauthenticated attacker with network access via multiple                 protocols to compromise Java SE, Java SE Embedded. Successful attacks of this vulnerability can result in unauthorized                 ability to cause a partial denial of service (partial DOS) of Java SE, Java SE Embedded.
Java CVE-2019-2964Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE                 (component: Concurrency). Difficult to exploit vulnerability allows unauthenticated attacker with network access via                 multiple protocols to compromise Java SE, Java SE Embedded. Successful attacks of this vulnerability can result in                 unauthorized ability to cause a partial denial of service (partial DOS) of Java SE, Java SE Embedded.
Java CVE-2019-2978Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE                 (component: Networking). Difficult to exploit vulnerability allows unauthenticated attacker with network access via                 multiple protocols to compromise Java SE, Java SE Embedded. Successful attacks of this vulnerability can result in                 unauthorized ability to cause a partial denial of service (partial DOS) of Java SE, Java SE Embedded.
Java CVE-2019-2983Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE                 (component: Serialization). Difficult to exploit vulnerability allows unauthenticated attacker with network access via                 multiple protocols to compromise Java SE, Java SE Embedded. Successful attacks of this vulnerability can result in                 unauthorized ability to cause a partial denial of service (partial DOS) of Java SE, Java SE Embedded.
Java CVE-2019-2989Vulnerability in the Oracle GraalVM Enterprise Edition product of                 Oracle GraalVM (component: Java). Difficult to exploit vulnerability allows unauthenticated attacker with network                 access via multiple protocols to compromise Oracle GraalVM Enterprise Edition. While the vulnerability is in Oracle                 GraalVM Enterprise Edition, attacks may significantly impact additional products. Successful attacks of this                 vulnerability can result in unauthorized creation, deletion or modification access to critical data or all Oracle                 GraalVM Enterprise Edition accessible data.
Java CVE-2019-2988Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE                 (component: 2D). Difficult to exploit vulnerability allows unauthenticated attacker with network access via multiple                 protocols to compromise Java SE, Java SE Embedded. Successful attacks of this vulnerability can result in unauthorized                 ability to cause a partial denial of service (partial DOS) of Java SE, Java SE Embedded.
Java CVE-2019-2992Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE                 (component: 2D). Difficult to exploit vulnerability allows unauthenticated attacker with network access via multiple                 protocols to compromise Java SE, Java SE Embedded. Successful attacks of this vulnerability can result in unauthorized                 ability to cause a partial denial of service (partial DOS) of Java SE, Java SE Embedded.
Java CVE-2019-2894Vulnerability in the Java SE, Java SE Embedded product of Oracle Java SE                 (component: Security). Difficult to exploit vulnerability allows unauthenticated attacker with network access via                 multiple protocols to compromise Java SE, Java SE Embedded. Successful attacks of this vulnerability can result in                 unauthorized read access to a subset of Java SE, Java SE Embedded accessible data.
Java CVE-2019-2996Vulnerability in the Java SE, Java SE Embedded product of Oracle                 Java SE (component: Deployment). Difficult to exploit vulnerability allows unauthenticated attacker with network access                 via multiple protocols to compromise Java SE, Java SE Embedded. Successful attacks require human interaction from a person                 other than the attacker. Successful attacks of this vulnerability can result in unauthorized update, insert or delete                 access to some of Java SE, Java SE Embedded accessible data as well as unauthorized read access to a subset of Java SE,                 Java SE Embedded accessible data.
Java CVE 2019-10086In Apache Commons Beanutils 1.9.2, a special BeanIntrospector                 class was added which allows suppressing the ability for an attacker to access the classloader via the class property                 available on all Java objects. However, this is not used by the default characteristic of the PropertyUtilsBean.
Java CVE 2019-12384FasterXML jackson-databind 2.x before 2.9.9.1 might allow attackers                 to have a variety of impacts by leveraging failure to block the logback-core class from polymorphic deserialization.                 Depending on the class-path content, remote code execution may be possible.
Java CVE 2019-14379SubTypeValidator.java in FasterXML jackson-databind before 2.9.9.2                 mishandles default typing when ehcache is used (because of net.sf.ehcache.transaction.manager.DefaultTransactionManagerLookup),                 leading to remote code execution.
Java CVE 2019-14439A Polymorphic Typing issue was discovered in FasterXML                 jackson-databind 2.x before 2.9.9.2. This occurs when Default Typing is enabled (either globally or for a specific property)                 for an externally exposed JSON endpoint and the service has the logback jar in the classpath.
Java CVE 2019-14540A Polymorphic Typing issue was discovered in FasterXML jackson-databind                 before 2.9.10. It is related to com.zaxxer.hikari.HikariConfig.
Java CVE 2019-16335A Polymorphic Typing issue was discovered in FasterXML jackson-databind                 before 2.9.10. It is related to com.zaxxer.hikari.HikariDataSource. This is a different vulnerability than CVE-2019-14540.

    

  

Issues fixed in version 08.1.00

   

      

  • You can find the problems, workarounds and fixes related to this release in the issue list.    

 

   

New features in version 08.1.00

    

       

  • New features:                             
    • You can protect the Edit Mode, when an edit mode password is assigned or the user management is active.               
    • Password change for the first time login on a device               
    • Forward events to a syslog server over TLS               
    • Configurable auto-acknowledge function, when the status changes for an event               
    • Generate test events when configuring status configuration               
    • Globally Enable/Disable monitoring of the Security Status               
    • Start HiProvision from Industrial HiVision               
    • Show number of selected list entries               
    • When configuring event actions, you can test the action during the configuration.               
    • Certificates are stored in a key store for sub-domain interfaces.               
    • The user can now reset the icon on multiple devices to the default icon, as long as there are only devices selected.            
  •               
  • New devices:                             
    • Hi-SCOM BN48 and BN3049                           
  • MultiConfig™ dialogs added:                             
    • Switching - MRP-IEEE - MVRP Configuration (HiOS)               
    • Switching - GARP - GMRP (HiOS)               
    • Switching - GARP - GVRP (HiOS)               
    • Switching - VLANs - Voice (Classic Software, HiOS)               
    • Routing - ARP - Global (Classic Software)               
    • Diagnostics - Email Notification - Global - Create Email Subject (HiOS)               
    • Diagnostics - Ports - Port-Mirroring (HiOS)               
    • Port Dialog: Port - Port Security (Classic Software, HiOS)               
    • Port Dialog: Port - Dynamic ARP Inspection (HiOS)               
    • Port Dialog: Port - MRP-IEEE - Configuration (HiOS)               
    • Port Dialog: Port - MRP-IEEE - MMRP (HiOS)               
    • Port Dialog: Port - MRP-IEEE - MVRP (HiOS)               
    • Port Dialog: Port - GARP - GMRP (HiOS)               
    • Port Dialog: Port - GARP - GVRP (HiOS)               
    • Port Dialog: Port - DHCP L2 Relay (HiOS)               
    • Port Dialog: Port - DHCP Server (HiOS)               
    • Port Dialog: Port - Profinet IO (HiOS)            
  •           
  • MultiConfig™ dialogs modified:                             
    • Routing - ARP - Global (HiOS, HiSecOS)               
    • Diagnostics - Email Notification - Global (HiOS)               
    • Diagnostics - Email Notification - Mail Server (HiOS)               
    • Port Dialog: Port - POE (Classic Software, HiOS)            
  •           

   


   

Additions to the manual in version 08.1.00

   

       

  •            The following sentence, "Industrial HiVision enters DeviceConfig_<IP-Adresse>, is changed to             "Industrial HiVision enters <IP-Address> in the File Name field".                
  •            In chapter "8.2.24 Properties of a component detail", section "Generate test events" (page 301):
               Ignore item 8 of the "Generate test events procedure":
               'In the "Import event" dialog, verify that the table displays the event for which you wish to assign an action'.             

   


    This version has been tested with the following firmware versions:

                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                             

DeviceFirmware version
BAT54RAIL8.80
BAT54RAIL-PLUS8.80
BAT-R9.12
BAT-F9.12
BAT-C2.3.8
BAT-2C08.02.01.02
BAT450-F9.12
BAT867-R9.12
Bobcat07.4.01
Dragon PTN2.4.52
Dragon MACH400007.4.00
Dragon MACH45007.2.02
DX940-2GSFP-4TX-4RS-T1-H4.0.0
DX1000-TS-02-H3.1.8
EAGLE RuggedizedHiSecOS-01.1.01
EAGLE RuggedizedHiSecOS-01.2.00
EAGLE RuggedizedHiSecOS-03.0.00
EAGLEONE-TX-TXONE-05.3.00
EAGLE20-TX-TXSDV-05.3.02
EES25-0600HiOS-2E-04.0.00
EESX20-0800HiOS-2E-04.0.00
EESX30-0600HiOS-2E-06.0.00
Gecko 4TX01.0.01
GRS1020-8T8ZHiOS-2S-06.0.00
GRS1020-16T9HiOS-2S-04.1.00
HiProvisionV04.0.14
IS30V011R021
LioN-RV1.0.10.8-1.4
MACH 30013.46
MACH 30023.46
MACH100L2P-09.0.12
MACH1000GEL3P-08.0.08
MACH4000 48GL3P-08.0.08
MACH4002-24GL2P-09.0.08
MACH4002-24G-3XL3P-09.0.04
Magnum 10RX4.0.4C1
MAR1030L2P-09.0.11
MAR1040L2P-09.0.12
MAR1040L3P-09.0.12
MS20-0800L2P-08.0.04
MS20-2400L2E-09.0.07
MS2108-24.06
MS30-0802L2E-09.0.07
MS4128-5L3P-09.0.07
MSP30-2404HiOS-2A-07.0.00
OCTOPUS 3HiOS-07.5.00
OCTOPUS-8ML2P-09.0.07
OS30-001604HiOS-2S-04.1.02
PowerMICEL3P-08.0.08
RED25-04002T1TTHiOS-2S-PRP-06.0.00
RS20-0400L2E-09.0.12
RS20-0800M2L2E-09.0.12
RS20-1600M2L2E-09.0.12
RS20-2500M3L2P-09.0.12
RS2-16M9.07
RS2-TX-TX9.07
RS30-0802L2P-09.0.12
RS30-2402L2P-09.0.12
RS40-0009L2P-09.0.12
RSB20L2B-05.3.05
RSP25-11003Z6ZTHiOS-2S-PRP-06.0.00
RSP35-08033O6TTHiOS-2S-06.0.00
RSPE32-24044O7T99HiOS-3S-04.0.00
RSR20-08TPL2P-09.0.12
RSR30-06TP-03COMBOL2P-09.0.12