BAT, WLC (HiLCOS)
-
How to give an Open BAT or a WLC an IP address ?
Pubblicato: Feb 9, 2018
Feb 21, 2018 -
First login (Password change) with LANconfig connecting the BAT device to a personal computer (2020-02-13)
Pubblicato: Feb 14, 2020
Feb 14, 2020 -
Wireless Point to Point Configuration Guide
Pubblicato: Dec 23, 2019
Dec 23, 2019 -
Roaming Parameters Infographic
Pubblicato: Feb 9, 2024
Feb 9, 2024 -
How to unlock weather channels
Pubblicato: Feb 21, 2018
Feb 21, 2018 -
How to optimize passive scan
Pubblicato: Feb 9, 2018
Jan 4, 2023 -
How to unlock channels 120, 124 and 128 in 5GHz subband 2 (when allowed by country regulation) ?
Pubblicato: Feb 9, 2018
Feb 9, 2018 -
How to set up 802.1x with EAP-TLS between Open BAT (as AP and Radius server) and Windows 7 client
Pubblicato: Feb 9, 2018
Nov 17, 2023 -
Howto configure a VPN between an OpenBAT and freeware Shrewsoft VPN Client (IPSec)
Pubblicato: Feb 9, 2018
Feb 21, 2018 -
How to resolve the hidden node problem
Pubblicato: Feb 9, 2018
Feb 9, 2018 -
How to store an alternate configuration
Pubblicato: Feb 9, 2018
Feb 9, 2018 -
How to use 802.11e (prioritization) on the Open BAT WLAN interfaces
Pubblicato: Feb 9, 2018
Feb 9, 2018 -
How to determine the managed Access Points behavior in case the controller fails
Pubblicato: Feb 9, 2018
Feb 9, 2018 -
How to configure VLANs in OpenBAT
Pubblicato: Feb 9, 2018
Jan 10, 2022 -
How to use the V.24 interface of an Open BAT as COM Port Server
Pubblicato: Feb 9, 2018
Feb 21, 2018 -
How to use a WLC as SCEP server and an Open BAT as SCEP client
Pubblicato: Feb 9, 2018
Feb 21, 2018 -
How to add a BAT or a WLC in LANconfig
Pubblicato: Feb 9, 2018
Feb 21, 2018 -
How to use an Open BAT or WLC as a RADIUS server and set up user accounts
Pubblicato: Feb 9, 2018
Jan 10, 2022 -
How to migrate a configuration from a Bat-54 to an OpenBat
Pubblicato: Feb 9, 2018
Feb 21, 2018 -
How to remotely capture the trafic of an Open BAT interface with RPCap function and Wireshark
Pubblicato: Feb 9, 2018
Feb 21, 2018 -
When a client roams from an AP to another one. How are the FDB of the switches behind the AP updated ?
Pubblicato: Feb 9, 2018
Feb 21, 2018 -
How to use Radius to access the BAT's agent
Pubblicato: Feb 9, 2018
Feb 21, 2018 -
How to redirect Broadcast when the BAT is used as router
Pubblicato: Feb 9, 2018
Feb 21, 2018 -
How to allow the 40MHz usage for channels 167-171 ?
Pubblicato: Feb 9, 2018
Feb 9, 2018 -
How to check the implemented settings for a country profile ?
Pubblicato: Feb 9, 2018
Feb 9, 2018 -
How to change the default config
Pubblicato: Feb 9, 2018
Feb 9, 2018 -
How to configure an Open BAT as an 802.1x supplicant
Pubblicato: Feb 9, 2018
Jan 10, 2022 -
How to configure an Open BAT as an 802.1x authenticator
Pubblicato: Feb 9, 2018
Jan 10, 2022 -
How to configure an Open BAT as Access Point
Pubblicato: Feb 9, 2018
Feb 21, 2018 -
How to configure an Open BAT as Access Client
Pubblicato: Feb 9, 2018
Feb 21, 2018 -
How to configure a Radius Profile on the WLC and include it in Logical settings
Pubblicato: Feb 9, 2018
Feb 21, 2018