When configuring a country in the HILCOS devices, a profile with different settings are automatically applied.
This profile take in account the WIFI regulations of the country (authorized channels, EIRP, use of DFS).
To check the settings automatically applied do the following:
- After configuring the country, log on the device per telnet
- Type "show wlan"
As output will be displayed the details of the profile applied
Ex for a device configured in USA:
admin@AP3:/
> show wlan
Channels Allowed By Regulatory Domain
=====================================
Country Setting: United-States-FCC
Indoor-Only Operation: No
Allowed Channels for 2,4 GHz Operation:
Channel(s) 1(2412 MHz), 2(2417 MHz), 3(2422 MHz), 4(2427 MHz), 5(2432 MHz), 6(
2437 MHz), 7(2442 MHz), 8(2447 MHz), 9(2452 MHz), 10(2457 MHz), 11(2462 MHz):
Allowed channel widths: 20MHz HT-40MHz
Tx power limit 28 dBm
EIRP limit 34 dBm
Allowed Channels for 5 GHz Operation:
Channel(s) 36(5180 MHz), 40(5200 MHz), 44(5220 MHz), 48(5240 MHz):
Allowed channel widths: 20MHz HT-40MHz
Tx power limit 14 dBm
EIRP limit 20 dBm
regulatory requirement(s):
indoor-only usage
Channel(s) 149(5745 MHz), 153(5765 MHz), 157(5785 MHz), 161(5805 MHz), 165(582
5 MHz):
Allowed channel widths: 20MHz HT-40MHz
Tx power limit 27 dBm
EIRP limit 33 dBm