Ir para o conteúdo principal

HiSecOS v04.3.02 released - Notícias / Firewalls - Belden Support Center

set. 7 2022

HiSecOS v04.3.02 released

Software Release 04.3.02
------------------------
Bugfixes (Refer Issue List)

Security Fix:
 - Kernel upgrade from v3.14.47 to v5.10.8
 - uclibc upgrade from v1.0.28 to v1.0.39
 - OpenSSl upgrade from v1.1.1d to v1.1.1n
 - expat upgrade from v2.2.0 to v2.4.7

Open points and decisions:
 - FDB: After adding static mac address to interface-1, same mac is getting learned to other interface-2 while traffic is send with same mac as source mac on interface-2
 - Eagle web become unresponsive, once web remain open for more than a day
 - After creating around 1000 L2 filter rule via CLI, web of L2 filter rule gives error to contact to manufacturer