This lesson describes how to configure the RADIUS Server function on an Open BAT or a WLC and set up user accounts.
You may need to refer to the following lessons for a complete working 802.1x environment (Supplicant - Authenticator - Server):
Environment without controller:
- How to configure an Open BAT as 802.1x supplicant
- How to configure an Open BAT as 802.1x authenticator
Environment with controller to manage the APs:
- How to configure an Open BAT as 802.1x supplicant
- How to create a profile on a WLC and apply it on BAT Acces points
- How to configure a Radius Profile on the WLC and include it in Logical settings
These How to are complementary and use the following settings for the radius authentication:
EAP - PEAP with MSCHAPv2 as tunnel method.
Representation
![](/file.php/6MHWRRDJNPP5452AEA57B/media_1417533224158.png)
A WLC or an Open BAT can be used as RADIUS Server.
The menus on both are identical but using a BAT the manual upload of a certificate is necessary (step described in this document).
Preliminary steps
Give the BAT an IP address (in our example: 192.168.1.150)
You can refer to the lesson "How to give an Open BAT or a WLC an IP address"
Add the BAT in LANconfig
You can refer to the lesson "How to discover a BAT or a WLC in LANconfig"
Upload a certificate on the server (if you use a BAT as RADIUS server)
![](/file.php/6BQSNQGNQCK5453AD4599/media_1418036976634.png)
This step is not necessary if you use a controller as RADIUS Server because the controller is able to generate its own certificates.
But, if you use a BAT then you have to do it manually. You'll need a certificate (.pfx or .p12 files, these files contain a private key and its associated certificate).
You can use for testing the attached file
SSL_certificates
(password for the certificates: hirschmann)
Then from LAN config, right clic on the BAT which has to be used as RADIUS server.
Configuration Management > Upload certificate or File ...
Select the .pfx or .p12 file you want to use and Select "EAP/TLS - Container as PKCS#12 file" as certificate type (it's usually protected by a password)
> Open
The file is uploaded on the BAT
Device status must be "OK" after the upload
General settings
![](/file.php/6SXMSWWCMST54541FF04C/media_1417534682567.png)
Configuration > RADIUS Server > General
Configure the authentication port: 1812
Configure the RADIUS clients list (Authenticators IP address and shared secret)
![](/file.php/6HQDGKMDTYD5455DA6724/media_1417534955672.png)
From the "General" dialog, select IPv4 clients
Create a new entry.
The new entry can be a single device (in our example it's only the device 192.168.1.140) but it could be a range of devices (the range is defined by the Netmask)
The shared secret will also be configured on the authenticator ( refer to the lesson "How to configure an Open BAT as 802.1x authenticator")
> OK
Set up User accounts
![](/file.php/6YXXTSRTJSH5456954F2E/media_1417535387284.png)
From the "General" dialog, select "User table"
Create a new entry for each user.
In our case we use just one user: laurent
To enter the name of the user and a password (in our case: lolothebest) is enough
The name and the password will be used by the supplicant ( refer to the lesson "How to configure an Open BAT as 802.1x supplicant")
> OK
After loading the configuration, your device is erady to be used as RADIUS server
Check the status of the NAS (Network Access Server or Authenticator)
![](/file.php/6ZYRZNDJSBY54571552F7/media_1418041614237.png)
You can check it via the web interface
HiLCOS Menu Tree > Status > TCP-IP > RADIUS-Server > Access-Control
Check the authentication of clients
![](/file.php/6RPSMZYXKHG5458CB7640/media_1418041905857.png)
You can see the result of the authentication tries in the Log-Table available via the Web interface under
HiLCOS Menu Tree > Status > TCP-IP > RADIUS-Server > Log-Table.
More information can be available if if we use RADIUS Accounting (not described in this How-to).