跳到主要内容

HiLCOS 10.12 Release Update 10 - 新消息 / Wireless - Belden Support Center

11月 2 2022

HiLCOS 10.12 Release Update 10


Hirschmann is proud to announce the release of HiLCOS 10.12 Release Update 10:

https://hirschmann-support.belden.com/en/downloads/files/hilcos-10-12-6924-release-update-10

HiLCOS device firmware version 10.12.

For the devices:

  • OpenBAT (BAT-F and BAT-R)
  • BAT450-F (all variants)
  • BAT867-R and BAT867-F
  • BAT WLC


Download also contains complementary software LANConfig and LANMonitor

Feature highlights as of version 10.12.6924 (Release Update 10)

Full list of new features can be found in the release notes in the zip file.

  • Make the PMK Lifetime configurable at WLC
  • SNMP variable for noise per chain
  • Default TLS encryption set to version 1.2. Older versions are still supported, but deactivated by default.

Bugfix highlights as of version 10.12.6924 (Release Update 10)

Full list of bugfixes can be found in the release notes in the zip file.

  • Security updates for TinyXML and OpenSSL
  • Rare connection drops between AP and WLC have been resolved