Zum Hauptinhalt springen

HiLCOS 10.34 Release Update 3 - Neuigkeiten / Wireless - Belden Support Center

Dez. 14 2022

HiLCOS 10.34 Release Update 3

Hirschmann is proud to announce the release of HiLCOS 10.34 Release Update 3:

https://hirschmann-support.belden.com/downloads/files/3754

For the devices:

  • OpenBAT (BAT-F and BAT-R)
  • BAT450-F (all variants, except LTE)
  • BAT867-R and BAT867-F
  • BAT Controller Virtual and BAT WLC


Download also contains complementary software LANConfig and LANMonitor

Feature highlights as of version 10.34.5725 (Release Update 3)

Full list of new features can be found in the release notes in the zip file.

Bugfix highlights as of version 10.34.5725 (Release Update 3)

Full list of bugfixes can be found in the release notes in the zip file.

  • Security updates
  • Singapore: U-NII-3 channels are now supported
  • Improved Client support when connected to Huawei Access Points